AXIS#.SAFEPARAM.SDIp.TIMEDELAYMONITORING

Description

Indicates the delay before starting the position and velocity monitoring when the Safe Direction positive (SDIp) safety function is activated.

 

Parameters Editor with Time Delay Monitoring (t_D_SDOp) circled

 

This value is called t_D_SDIp.


  • The timers t_D_SDIp and t_D_SDIn are not shown in this picture below due to clarity. The behavior of the timers is similar to the timer t_D_SOS shown in the function SOS. In the image the timer t_D_SDIn runs at times t1 and t13. The timer t_D_SDIp runs at the times t6 and t13.

 

Context

For complete SDI information refer to SDI (Safe Direction)

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Milliseconds

Range

[1, 60000]

Default Value

1

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SDIP.TIMEDELAYMONITORING

3164h

06h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SDIP.TIMEDELAYMONITORING

3264h

06h

Unsigned16

-

-

Read/Write

No